|     RoHS     |     VIEW RFQ     |     DIGI-KEY INVENTORY     |     CONTACT     |     COMPANY     |     PRESS ROOM     |
PRODUCT SEARCH: 
 
   
PRODUCTS
 

RoHS Statement

In response to the legislated environmental directives being instituted throughout the world, CUI has established a comprehensive program that is intended to promote product compliance with the new laws. At this time, the key environmental directives are from the European Community, with many countries/states either following these directives explicitly or instituting their own variations. The most notable directive is the RoHS (Restriction of the use of certain Hazardous Substances). The RoHS legislation restricts the use of certain hazardous substances to levels of less than 100-1000 ppm used in electronic products. The RoHS and equivalent directives prohibit use of the following substances in products placed into the market effective July 1, 2006:

· Lead · Hexavalent Chromium
· Mercury · Cadmium
· Polybrominated Biphenyls (PBB) · Polybrominated Diphenylethers (PBDE)

CUI has received requirements from many customers to provide products conforming to these environmental regulations. In order to serve our customers, we are in the process of ensuring that 100% of our products are compliant with the RoHS directive. Currently 98% of CUI products are RoHS compliant with the remaining 2% scheduled to become compliant by July 1, 2006.

All CUI RoHS compliant parts are compatible with lead-free solder processes.

Part specific RoHS information, including a RoHS Certificate of Compliance, is available on the website. The website will continually be updated as parts become compliant and when additional RoHS information is available. If you can not find the RoHS information that you need on the website, please contact CUI directly at 800-275-4899.


RoHS information on the website:

To make finding RoHS compliant parts easier, CUI has designated a logo to indicate which parts are compliant.


The logo displays in the following locations:


Product Search results


Specification sheets


RoHS certificates of compliance

 
 

CUI Inc., 20050 SW 112th Ave., Tualatin, OR 97062 • FAX: 503.612.2383 • 800.275.4899
© 2003 - 2010 CUI INC, All Rights Reserved. Privacy Policy   Terms/Conditions   Site Map   Home  
THIS SITE BEST VIEWED IN IE 5.5+