The Adoption of IEC 60601-1 Around the Globe (Infographic)

October 31, 2017 by CUI Inc

The IEC 60601-1 standard, which provides general requirements that address the basic safety and essential performance of medical electrical equipment, has evolved through a number revisions since its first publication in 1977. Keeping on top of these revisions and new editions of the standard has proven to be a challenge for medical device designers because of their many regional variations and differing adoption timelines around the globe.

With the introduction of collateral standard IEC 60601-1-2 (“Electromagnetic disturbances – Requirements and tests”) in 2014, now commonly referred to as the “4th edition,” the global landscape has become even more unclear. To help illustrate the adoption timeline of IEC 60601-1 as it relates to various territories worldwide, we have developed this country compliance infographic that highlights the evolution of the different editions now and into the future.

The Global Adoption of IEC 60601-1

Helpful Resources

For more information on the IEC 60601-1 medical design standards and regional compliance timelines, check out our in-depth application note

View our full line of medical 60601-1 4th edition compliant power supplies

Have comments regarding this post or topics that you would like to see us cover in the future? Send us an email at techinsights@cui.com


TODO: tags & categories
CUI Inc

CUI Inc

As a leader in power electronics and electromechanical components, we strive to provide engineers with reliable and proven solutions across a range of market segments as technology allows the world to connect in new ways. Most importantly, we have an unwavering commitment to create collaborative partnerships with customers and to equip them with the tools and resources they need to succeed.