The Power of Things™

With the rapid rise of the Internet of Things, trillions of sensors will enter the market and zettabytes of data will flow through our server infrastructure. This creates new power challenges across all industries and applications. Learn how CUI is supporting The Power of Things, so you can design for the Internet of Things.

▶ The Power of Things

 

News & Events

 

CUI Announces Partnership with Virtual Power Systems

CUI Inc and its parent company CUI Global, Inc. (NASDAQ:CUI), announced a limited exclusivity agreement today for hardware development with Virtual Power Systems (VPS), a cutting edge Software Defined Power® company. The companies will partner to set a new standard for an efficient power infrastructure for data centers.

With this agreement, CUI will design, manufacture, and distribute the hardware component of the ICE (Intelligent Control of Energy) system that realizes the full value of the VPS solution. This partnership between the two organizations is the first step in creating a larger Software Defined Power ecosystem, from board level to system level, ultimately creating a more intelligent, more efficient data center infrastructure.

▶ Learn More

 

Is Your Power Supply Level VI Compliant?

On February 10, 2014, the U.S. Department of Energy (DOE) published a revision to its EISA 2007 external power supply (EPS) efficiency standard increasing the minimum efficiency requirements as well as expanding the range of products applicable under the new standard. Set to go into effect February 10, 2016, this law will have implications for any OEM that designs products with an external ac-dc power supply for the US market. To keep you one step ahead, CUI is developing a robust portfolio of Level VI compliant external ac-dc adapters utilizing the latest in green power technology.






▶ Learn More

 

New Products

Level VI Wall Plug Ac-Dc Power Supplies Designed to Meet Tightened Efficiency Regulations

The SWI6, SWI12, SWI18 and SWI24 are wall plug-in ac-dc power supplies with either North American or European input blades designed to meet the new Level VI efficiency standards. All models boast no-load power consumption less than 0.1 W and feature a range of safety approvals in CUI's effort to provide customers with the latest in green power technology.

  • Level VI efficiency
  • NA or EU input blades
  • No load power consumption < 0.075 W
  • Universal input voltage range
  • Over voltage, over current, and short circuit protections
  • UL/cUL, PSE, and CE safety approvals

SWI6-N Series / SWI6-E Series / SWI12-N Series / SWI12-E Series / SWI18-N Series / SWI18-E Series / SWI24-N Series / SWI24-E Series

1100 W Front-End Power Supply Series Expanded to Include Dc Input Versions

The PSD-1100 is an 1100 W hot-swappable front-end dc-dc power supply packaged in a slim line 1U case. Featuring Platinum efficiency, PMBus communication and N+1 redundancy, this 12 V dc power supply is ideal for mission critical telecom, server and networking applications requiring a dc input.

  • Up to 1100 W continuous power
  • 80 PLUS Platinum Efficiency
  • High power density - 25.34 W/in3
  • Slim line 1U form factor
  • PMBus communication for monitoring and control
  • Front to back (-F) and back to front (-B) airflow versions
  • Redundant (N+1) operation
  • Blind mate connections for hot-swap functionality
  • DROOP current sharing
  • Remote on/off control
  • Power good signal
  • Options:
    • 3.3 V or 5 V standby voltage
    • Forced current share

PSD-1100-12 Series

Resources

In this article published by EDN, Mark Adams, CUI's Senior VP, discusses the continued pressure that our data-centric lifestyles have put on our power infrastructure. The article further outlines the demand for power, the move to software-defined power and how the rapidly adopted technology is put into practice.

Read It Now

In this article published by Electronic Design, Aaron Yarnell, CUI's Field Applications Engineering Manager, highlights ten points to look for in a POL module in order to keep up with the rapid change in voltage, current, power and switching speed requirements.

Read It Now

Contest

Level VI External Ac-Dc Power Supplies

CUI's current line of Level VI compliant external ac-dc adapters are available in desktop and wall plug versions while offering no load power consumption as low as < 0.075 W, a universal input voltage range and UL/cUL, GS and PSE safety approvals, keeping users one step ahead of the more stringent US regulations on external adapters.

Question: What is the universal input voltage range for CUI's line of Level VI adapters?

Submit your answer to contest@cui.com.

(One winner will be selected on 02/01/2016 and notified via email.)

20050 SW 112th Avenue
Tualatin, OR 97062
1-800-275-4899
www.cui.com