Power Blog Homepage

What are the Differences Between IEC Power Supply Protection Classes?

August 4, 2020 by Bruce Rose - 4 Minute Read

What are the Differences Between IEC Power Supply Protection Classes?

The International Electrotechnical Commission (IEC) has defined three safety classes for power supplies: Class I, Class II, and Class III. These three classes are used to identify different methods for preventing the user of the power supply from being subjected to hazardous voltages from the input power source. Although it is easy to understand the differences in the IEC classes, many engineers are not familiar with the definitions and thus this blog will present a quick explanation of the differences between the classes.

  1. Class I - a layer of basic insulation and a grounded conductive chassis
  2. Class II - double insulation (basic + supplemental) or reinforced insulation
  3. Class III - no protection needed as the input voltage is not hazardous

Class I Power Supplies

In IEC Class I power supplies the user is protected from hazardous input voltage levels by at least a layer of basic insulation and a grounded conductive chassis. The first level of safety protection is provided by the basic insulation. The second level of safety protection is provided by the grounded conductive chassis. If there is a failure of the basic insulation, then any conductor with a hazardous voltage will be grounded by the conductive chassis before the hazardous voltage can come in contact with the user. All Class I power supplies must have safety ground brought to an electrically conductive chassis in the power supply.

Diagram of Class I power supply requirements

Class II Power Supplies

In IEC Class II power supplies the user is protected from hazardous input voltage levels by at least a layer of basic insulation and a layer of supplemental insulation or a layer of reinforced insulation. For double insulation, the first level of safety protection is provided by the basic insulation while the second level of safety protection is provided by the layer of supplemental insulation. Reinforced insulation provides the same safety factor as the combined basic and supplemental layers of insulation but in a single layer of insulation. For more on insulation check out our blog post on Insulation, Isolation, and Working Voltage.

Because of double or reinforced insulation, IEC Class II power supplies are not required to have the safety ground conductor brought to the power supply.

Diagram of Class II power supply requirements

A common source of confusion is the difference between an IEC Class II power supply and a NEC Class 2 power supply. This topic is covered in our post What's the Difference Between Class 2 and Class II Power Supplies?

Class III Power Supplies

In IEC Class III power supplies the input voltage is not at a hazardous level and thus the user does not need to be protected from the input voltage. The IEC label for the non-hazardous input voltage is Safety Extra Low Voltage (SELV). The voltage in accessible parts of SELV circuits shall not exceed 42.4 Vac peak or 60 Vdc for longer than 200 ms., with an absolute limit of 71 Vac peak or 120 Vdc. SELV circuits must be separated from hazardous voltages by two levels of protection. The two layers of protection may be basic and supplemental insulation, reinforced insulation, or basic insulation combined with a safety grounded electrically conductive chassis.

Diagram of Class III power supply requirements

Understanding the three IEC Power Supply Protection Classes enables those specifying or selecting power supplies to choose the appropriate class of supply based upon safety, regulatory, and cost constraints.

Categories: Fundamentals , Product Selection

You May Also Like


Have comments regarding this post or topics that you would like to see us cover in the future?
Send us an email at powerblog@cui.com

Bruce Rose

Bruce Rose

Principal Applications Engineer

During his many years in the electronics industry working in design, sales, and marketing, Bruce Rose has focused on analog circuits and power delivery. His range of work experience includes organizing and chairing international workshops, publishing and presenting in more than 40 technical conferences and journals, and having been awarded seven patents. While he enjoys his time at work, Bruce further enjoys the time he is able to spend with his family hiking, biking, and canoeing as well as pursuing his passion of full scale and model aviation.

Need More Info?

Like this blog post?

Sign up to get the latest articles straight into your inbox.


Privacy Policy

This site is protected by reCAPTCHA and the Google Privacy Policy and Terms of Service apply.

*Note: Newsletter is currently only available in English.