Architects of Modern Power (AMP) Consortium Announces its First Set of Standards for Distributed Power Systems

11/12/2014


Architects of Modern Power (AMP) Consortium Announces its First Set of Standards for Distributed Power Systems

The newly formed Architects of Modern Power (AMP) consortium today announced its first standards aimed at establishing common mechanical and electrical specifications for the development of advanced power conversion technology for distributed power systems. The initial standards revealed at electronica, and being demonstrated by AMP Group products on show at CUI’s booth (B2-113), cover digital point-of-load (POL) and advanced bus dc-dc converters.

The goal of the alliance between CUI, Ericsson Power Modules and Murata is to realize the most technically advanced, end-to-end solutions and provide a complete ecosystem of hardware, software and support. Beyond purely mechanical specifications, it is the standardization of monitoring, control and communications functions, and the creation of common configuration files for plug-and-play interoperability that will ensure compatibility between each firms’ products.

Two standards have been defined for digital point-of-load converters. The ‘microAMP’ specification covers supplies rated at 20 to 25 A in vertical and horizontal configurations, while the ‘megaAMP’ defines requirements for 40 to 50 A vertical and horizontal units. For advanced bus dc-dc converters the ‘ABC-ebAMP’ standard relates to advanced bus bricks measuring 58.42 x 22.66 mm and ranging from 264 to 300 W. For quarter-brick supplies, measuring 58.42 x 36.83 mm and ranging from 420 to 468 W, the Group has defined the ‘ABC-qbAMP’ standard. These standards detail mechanical footprints, features, and configuration files.

AMP Group spokesperson and CUI VP of Advanced Power, Mark Adams, commented, “Following the launch of Architects of Modern Power last month, the release of these standards marks an important first step on our shared technology roadmap.” Patrick Le Fèvre, Marketing Communications Director at Ericsson Power Modules said, “Providing a true multi-sourced, high efficiency power ecosystem with exceptional supply chain reliability enables continuity of production for our customers,” while Murata Power Solutions’ VP of Strategic Product Marketing, Steve Pimpis, added, “We are excited to make this advanced technology available in a way that allows wider adoption than would be possible with single-source solutions.”

Products meeting these standards are available now from the AMP Group and will be on display at electronica in Munich, November 11-14th, 2014 (CUI booth B2-113, Murata booth B5-107, Ericsson Power Modules at the MEV booth A4-260).

For more information, visit www.ampgroup.com